2023-01-17 1:02 PM
2023-01-18 2:53 AM
Hello @vVukm.1
Could you further explain the issue please?
Are yo using STM32CubeMX or STM32CubeProgrammer ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-19 1:16 PM
I'm using STM32CubeIDE and STM32CubeMX and CUBE STM32CubeProgrammer
and in any of this programs I 'cant select target STM32F723IEK6.
2023-01-19 5:53 PM
Reposting the same information doesn't advance the conversation.
Perhaps show STM32 Cube Programmer connecting with the ST-LINK/V3SET, and the STM32F723 MCU on *YOUR* board.
Are you talking about the STM32F723IEK6 that provides the ST-LINK functionality? Don't expect to be programming that.
2023-01-21 12:19 PM
2023-01-21 12:47 PM
What is the ST-LINK/V3SET connected too?
The ST-LINK should be connecting to some STM32 device on a board you attach it too.
Diagram what you're doing
2023-01-22 10:55 AM
Hello @vVukm.1,
It looks like your ST-LINK device is not being detected. There are a few things you can try to fix this issue:
Also what board are you using exactly?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-24 12:25 PM
2023-01-24 12:29 PM
you did not answer:
> What is the ST-LINK/V3SET connected too?
+
>The ST-LINK should be connecting to some STM32 device on a board you attach it too.
Diagram what you're doing !
what you want - if not show, what your doing ?
2023-01-25 10:37 AM