2019-01-19 03:28 AM
Hello!
I cannot install STM32 ST-LINK Utility v4.3.0 setup, error(attach screenshot).
I Use Windows 10 64bit.
Can who experienced such a pain? From whom normally works STM32 ST-LINK Utility running Windows 10?
2019-01-19 06:47 AM
Run installer "As Administrator" or check other options/policies that might preclude installation, ie external USB device. Determine if AV software is interfering with machine operation.
If this is a managed PC have the "IT" people review settings/logs.