2020-07-12 11:43 PM
2020-07-13 12:28 AM
Hello,
Since the nucleo already has the debuger embedded, I suggest using a USB isolator between the PC and the nucleo.
Something like Adafruit USB isolator, which works fine as long as your device does not need more than 100mA.
2020-07-13 02:01 AM
@Kraal Yes I am looking for that option also, but it would be an advantage to know if there is anything like st-link available for this type of board.