cancel
Showing results for 
Search instead for 
Did you mean: 

10-pin debug connector and STLINK-V3-ISOL - not reliable?

PHolt.1
Senior III

I am using STLINK V3 with the ISOL board, and using the supplied 10-core cable, going to this connector in my 32F417 target

https://peter-ftp.co.uk/screenshots/202105072011602908.jpg

On the target connector, I have pins 3,5,7,9 grounded.

Pins 2,4,6,10 go to CPU pins PA13,PA14,PB3,PB4.

It works, but reliably only for code download. If I try to run SWV ITM data console, that also works but very soon I get a loss of comms. I am running at 8MHz; the ISOL debugger can go up to about 15MHz before it fails. I tried it at 1MHz but the same happened.

The wires to the CPU are pretty short - 5cm max.

I would be grateful for any ideas.

Console output:

------ Switching context -----

Target connection mode: Default

Reading ROM table for AP 0 @0xe00fffd0

Hardware watchpoint supported by the target

Failed to set com freq, status 0

COM frequency = 8000 kHz

ST-LINK Firmware version : V3J7M2B4S1

Device ID: 0x413

PC: 0x8025688

ST-LINK detects target voltage = 3.25 V

ST-LINK device status: HALT_MODE

ST-LINK device initialization OK

SWV_SetStatus(true): stop_reply_pending == 0

handle_vCont_c, continue thread

ST-LINK device status: RUN_MODE

ST-LINK device status: HALT_MODE

SWV_SetStatus(false): stop_reply_pending == 1

TraceCaptureStart and SWV event set to APP_FALSE (0)

NVIC_DFSR_REG = 0x0000000A

SWV_SetStatus(true): stop_reply_pending == 0

handle_vCont_c, continue thread

ST-LINK device status: RUN_MODE

ST-LINK device status: Failed to get status, Target not responding, retrying... 19

Target is not responding, retrying...

ST-LINK device status: Failed to get status, Target not responding, retrying... 19

Target is not responding, retrying...

ST-LINK device status: Failed to get status, Target not responding, retrying... 19

Target is not responding, retrying...

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PHolt.1
Senior III

As usual, nobody answers.

Anyway, I solved it. There seems to be a fault on the MB1440B board, when stacked on top of the MB1599B board (the ISOL board). The 20-way connector works but the 14-way (CN1, which is used for the 10-way cable) does not. Well, it works but with a lot of intermittent faults. The solution is to not use MB1440B and plug the 10-way cable into the MB1599B board instead (CN1 also).

Imen.D
ST Employee

Hi @PHolt.1​ ,

I added this thread to your post as contains the same topic, and this will help other users find that discussion faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen