2023-05-26 2:27 AM
should i connect external power supply to flash the program.
when i connect ST-LINK/V2 to PCB board i get the error called "no cortex-m device found".
"no target is connected".
Please anyone help me to flash the program to my customised pcb board.
2023-05-26 2:28 AM
in the above pin it is JTMS
2023-05-26 3:09 AM
If the CPU is not powered by the st-link, then you need to power it by external power supply.
2023-05-26 3:19 AM - edited 2023-11-20 4:31 AM
from the ST-LINK
This is the connection
2023-05-26 5:12 AM
Check on board: is CPU vdd 3.3 V ?
And connect: software reset mode .