2023-03-24 06:21 AM
I am facing a problem while programming a board the arduino ide is unable to Detect the board and giving this error.
and my Arduino ide Board Configuration are
But in Device Manager it detecting problem as shown below.
and my board configuration are as shown below
Please help me to resolve this. and also can you provide my knowledge about how to program this same nucleo board with ST Link
2023-03-27 01:26 AM
Hello @ASing.28 and welcome to ST Community,
I can't seem to see an issue with your installation since you can see the board and the COM in the Arduino IDE, make sure you have followed all the steps here.
If this is the first you are trying stm32duino, problems generally occurs due to a misconfigured proxy, a blocking by a firewall or an intolerant antivirus
Regarding you last question, do you mean programming your Nucleo with ST Ecosystem
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-27 01:34 AM
Thank you ! It is resolved. I was using different board.