cancel
Showing results for 
Search instead for 
Did you mean: 

how to get the official Firmware of the debugger STLINK-V2-1?

MDowa.1
Associate

Hello everyone,

i am planing to use an STM32 microcontroller in a project and would like to have a debugger on the same board. I then have to use another microcontroller ie. STM32F103CBT6 the same as used on STLINK-V2-1 on Nucleo boards, which will act as the debugger for the actual microcontroller. But this need to be flashed with the right firmaware to do its job.

I have searched everywere for an original firmware of STLINK-V2-1 but did not find any. How can i find an official and original Firmware for STLIN-V2-1 debugger?

Thanks alot!

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @MDowa.1​, to the community!

The firmware for the ST-LINK is not available for self-building of the ST-LINK and is legally programmed exclusively on original ST-LINKs.

However, you can solder in the STLINK-V3MODS, which were developed directly for this purpose.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

Welcome, @MDowa.1​, to the community!

The firmware for the ST-LINK is not available for self-building of the ST-LINK and is legally programmed exclusively on original ST-LINKs.

However, you can solder in the STLINK-V3MODS, which were developed directly for this purpose.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MDowa.1
Associate

Hi Peter,

thanks for fast answering.

Ok i see. Using the STLINK-V3MODS is then the best idea.

Again thank your very much! 🙂

You're welcome.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Paul1
Lead

<<Ignore this, appears to actually be PC side code, not STLink Firmware :(

Is this "Open Source STLINK" on Github OK to use?