2024-02-09 10:39 PM
Hello!
I'm starting a project where I need to read several external analog signals simultaneously. The reference manual of the STM32F469I-DISCO states that its ADC has up to 16 channels to measure analog signals. However, upon reviewing the schematic of the board, I realized that there aren't enough physical connectors for the ADC channels (or at least that's what I found—I'm still a beginner). Is there any way to solve this problem, such as using an external module or board?
I appreciate your responses and assistance very much.
2024-02-10 12:07 AM - edited 2024-02-10 12:08 AM
Hello @Danodino and welcome to the ST Community 😊.
the STM32F469I-DISCO is based on the STM32F469NIH6 MCU wish (according to the DS11189) give you the opportunity to use 24 ADC channel on the same time:
If you are looking for more ADC channels, you can even look for another MCU that support more channels (ST-MCU-FINDER-PC may help you). Or you can use an external ADC to SPI converter that add some ADC channels throw SPI interface.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-10 01:49 AM - edited 2024-02-10 01:51 AM
@Danodino wrote:The reference manual of the STM32F469I-DISCO states that its ADC has up to 16 channels to measure analog signals.
You mean the User Manual, UM1932?
I don't see "16 channels" mentioned in there?
@Danodino wrote:However, upon reviewing the schematic of the board, I realized that there aren't enough physical connectors for the ADC channels
That's the trouble with a development board like that - which has a loads of accessories bolted on:
All of those things use up processor pins - meaning they're not free for you to use for other things.
If you want maximum unobstructed access to as many of the chip's pins as possible, you want a dev board with as few "extras" as possible.
So you'd be better looking at a Nucleo board - they are pretty minimalistic in terms of the "extras":
https://www.st.com/en/evaluation-tools/stm32-nucleo-boards.html
2024-02-10 04:10 AM
Hi,
STM32F469I-DISCO has some ADC inputs on connectors, you can use:
So you have : 6 x adc in on CN8 , some (4x) on CN5+7 : PA1/2/6/7 , (2x) on CN12 : PA5 , PC1 ; 12x i found.
maybe more, just look in ds pinouts for all pins on the headers.
How many you need ? + you have all the opamps+circuit to bring clean 0...3v3 signals to the inputs ?
2024-02-11 04:01 PM
Hello again,
Thank you very much for replying, @AScha.3. 🙂
Being optimistic, I need to read 12 signals (I'm developing a system for electrocardiography recording), but I can reduce it to only 6 signals if necessary.
I found the ones you mentioned on CN8 and CN12, but I don't know how you identified the 4x from CN5 and CN7; there is no label related to ADC channels (it would be awesome if there are actually 12 available channels). Could you explain how you figured them out?
@AScha.3 wrote:
How many you need ? + you have all the opamps+circuit to bring clean 0...3v3 signals to the inputs ?
My analog circuit is supplied with a symmetric source of ±12V. My outputs are supposed to be in the -1.5V to 1.5V range, but there isn't any extra circuit that ensures my output won't be greater than 3.3V and less than 0V. Now, I realize that I have to add that to my PCB and make the pertinent modifications (thank you for that).
2024-02-11 11:46 PM
Hi,
Let your book of wisdom be the manual .
Here it is the ds and the rm , about 1800 pages, and the board circuit diagram .
In circuit diagram you see, what pins you could use to connect ,
and in ds look in pin definitions, whats on these pins: looking for ADC inputs you see, they are on some group of pins:
So PA1/2/6/7 can be switched to adc inputs ...
Now : what you should do , to go on ->
Use the comfort, the stm32CubeIDE or CubeMX offers you:
Start new stm32-project, select your 469-disco board and give a name and let it work some minutes...
then have a pinout picture, where you can see whats connected and change/set the analog inputs you want to the ADCs . Then generate code and you can start programming .
And if you have a problem...someone (me?) will show you how to do.
2024-02-12 02:37 AM
@Danodino wrote:I'm developing a system for electrocardiography recording
I'd be doubtful that this Disco board is optimised for low-noise on its analogue inputs ...