2023-11-27 5:38 AM
Hi,
I am not a pro user of using stm32 microcontrollers and i need to know if it is possible to connect an electret microphone with a stm32 nucleo h743zi board and see any information i receive with this component.
For example, i want to connect the condenser mic with nucleo board and see in my screen any data, or something to prove that i am connecting this correctly or know how to treat with these type of components.
This photo shows the type of condenser microphone i am using.
Sorry if i am not explaining it so well because i don't know if it is possible to do things like i am asking here.
Thank you so much for your time.
2023-11-27 6:49 AM
Yes, you can do that.
BUT...
1) Audio signal quality will be much worse than nowadays audio standard, due to the STM's 12-bit SAR ADC (or 16-bit?).
2) it's a loooong and hard way from having the components to actually getting any usable data to your PC.
Depending on your knowledge / skill level, this can take from 2 weeks (HW & STM pro with USB knowledge) up to several months.
3) Something many people forget: you need some software on the PC side as well.
2023-11-27 10:31 PM
Thanks for answering,
> 1) Audio signal quality will be much worse than nowadays audio standard, due to the STM's 12-bit SAR ADC (or 16-bit?).
That's not a problem because in a future i will use other PCM4220PFBG4 (Audio converter) to fix quality. But first i want to know how to do simple things...
> 2) it's a loooong and hard way from having the components to actually getting any usable data to your PC.
Depending on your knowledge / skill level, this can take from 2 weeks (HW & STM pro with USB knowledge) up to several months.
It's okay to work long time, i need to know how to do this type of things so my main difficulty is to find how to start doing this kind of things. So where could i start to understand something about how to convert this data or where to plug the mic, or whatever ?? I'm a bit lost in here.
> 3) Something many people forget: you need some software on the PC side as well.
Apart from using stm32cubemx or stm32cubeIDE? Do you mean just to work with audio data?
Thank you so much!
2023-11-27 10:53 PM
2) Okay, you could start by connecting a 3.3 V electret to the STM ADC. Quite simple, the microphone datasheet basically shows how to do that.
3) I mean how to work with "audio data".
If it's your own simple data stream (e.g., USB virtual comport), you need to handle that on the PC side with some self-made software.
If you make your STM32 look like a USB audio device, PC side gets simpler, but STM32 side will be much harder.
2023-11-27 11:23 PM
And it is possible to see any data directly from a tera term using usart connections?
The main problem of doing the things you are telling is where to start..., I need to see any documentation or something to start, what can i read or watch to learn about this?
Thank you
2023-11-28 5:37 AM
Sure, you can send audio data via UART - and with some experience you can even see the sine in the numbers ... ;)
Starting: get a Nucleo board and do it.
2023-11-28 5:42 AM
I already got the nucleo board but not the knowledge :face_with_tears_of_joy:
2023-11-28 7:37 AM
At least something!
There are so many tutorials out there for STM32, lots of example source code, it just takes time and effort.
2024-02-28 3:43 PM
can you please share some examples source code or any link/video tutorial for STM32 connect to MEM microphone or audio
thank you !!