cancel
Showing results for 
Search instead for 
Did you mean: 

Hola Buenos dias. Acabo de adquerir un stm32 v3 pack el dia 14/02/2023 al que, no soy capaz de hacerlo conectar y me da fallo.

Bbarr.1
Associate III
21 REPLIES 21
Bbarr.1
Associate III

Hello, I have been reading the note AN2606, for my micro stm32f723 I understand that I have to use art 1 and 2.

I understand what you mean but my knowledge is very basic.

I'm going to leave it for j-tag mode for any micro that may have st.

I find it complicated because, even reading the informative note in the stmbox, I don't know which is the section to be able to configure the bit ports

Thank you very much for your attention

imik786
Associate

aquí hay algunas soluciones posibles para probar:

Vuelva a verificar las conexiones de hardware.

Verifique la fuente de alimentación: asegúrese de que la placa STM32 esté recibiendo suficiente energía.

Compruebe la configuración de programación y depuración.