2022-03-19 02:54 AM
2022-03-19 06:35 AM
The change should be made in the Windows INF file used to install the DFU driver (ST's or custom).
Unfortunately any change will invalidate the signature on the driver package, and obtaining a new signature is a pain. At least you can use the "Zadig" hack (see here).
2022-03-19 06:53 AM
I managed to change the device name and Windows recognizes the new one but device manager shows an error -> see attached picture.
Also, the "Events" tab in USB Input Device Properties says "Device xxxxxxxxx was not migrated due to partial or ambiguous match."
Thank you for answering, I would really like to get this problem solved.
2022-03-19 12:45 PM
What have you changed? where?
2022-03-21 02:42 AM
2022-03-21 07:34 AM
Sorry then I misunderstood your question. I thought you want a DFU device. Actually it looks like HID. Windows says that your HID descriptor is malformed. Try to find the error.
The answer for the device name visible in Windows is still the same.