2024-05-15 1:08 AM - edited 2024-05-15 1:37 AM
Hello everyone,
I am configuring an STM32F401RE and its RTC on the STM32CubeIDE software
I've written an program that debug without errors. But ErrorHandler() is called during the RCC Oscillators initialization (during the "SystemClock_Config(void)" process).
I think i'have followed the steps and the right parameters, but would you have a clue of where could it be from ? Let me know if you need additional pictores of the system configuration of the .ioc file maybe
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler(); //the call of ErrorHandler() happens here
}
Solved! Go to Solution.
2024-05-15 5:38 AM
2024-05-15 5:39 AM
And of course i have a screen that is meant to display the hour, but this one is only displaying black squares, i suppose this is related
2024-05-15 5:41 AM
I am currently working in a company and this is a test borad we have to try all the programs before implent them IRL, so I don't have any teacher or supervisor to check on me :(
2024-05-15 7:14 AM
Do you not have colleagues who could help?