cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to start GDB server

Franckeno
Associate

Hello, I have been trying for a while to test the STMCube programming chain up to the STM32F411 via the STLink without success despite all the ideas read in the forum. During a review of the requirements for the installation of CUBE it is noted, under Windows, WIN 7, 10 but not 8 or 8.1. Too bad, 8.1 is my OS. I attach the error message that it returns to me systematically. Thanks for your help !

Error in final launch sequence: Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (17) Could not find an ST-LINK with serial number 310061000E00004637364D4E.

Please verify the serial number in the debug c

PS: the serial number is the same as the one present when opening STM32 LINK utility

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mike_ST
ST Employee

Hello

It is an STM32F411 Discovery board ?

Can you connect to the F411 with the ST-Link Utility ?

Franckeno
Associate

Hello, no I am using STM32f411 black pill. And yes I can connect without problem with STM Link utility. Have a nice day and thank you