2018-10-08 2:55 AM
Hi,
I’m developing and external loader for ST-Link Utility and STM32CubeProgrammer.
My constrains/ requirements are:
I used (started from) the source code from STM32CubeProgrammer and the document UM0892.
After a lot of attempts I have a version/FW that run on STM32CubeProgrammer, and I’m able to erase, write and read the external flash.
The issues are:
1) Sometimes connecting, disconnecting and reconnecting the STM32CubeProgrammer to the ST-Link/v2 I receive this error::
“Error: flash loader C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/ExternalLoader/EN25Q40_MT447 cannot be loaded.�?
This if and only if a I erase or write the external flash before disconnecting and reconnecting, If a only read the external flash the error doesn’t arise (I can disconnecting and reconnecting without problems) . If I don’t disconnect the ST-Link/v2 all work fine i.e. I’m able to write, erase and read many times the external flash.
2) The same binary module (.stldr) that I use on STM32CubeProgrammer if used with ST-Link Utility doesn’t work, in detail, the ST-Link Utility load the model without error, I can erase the external flash (mass erase, sector erase) and also I can read the external flash (the read is more slowly than STM32CubeProgrammer ) but the write operation fails, and example log is:
11:27:27 : Erasing external memory success.
11:29:07 : Timeout during flash programming
11:2 9:07 : Error occured during program operation!
11:29:29 : Unable to run On-Chip verification!
11:29:38 : External memory program canceled
Someone can help me to understand these issues or suggest me a way to debug the FW/module?
Thanks.
Gianluca Costa
2018-10-08 3:34 AM
The ST-LINK Utilities are not receiving development efforts and have their own bugs and shortcomings.
Diagnosis of issues can be via telemetry on the serial port. Code should be tested independently within your own test framework before integration.