cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 uses SDMMC1-eMMC as external memory, how to configure the address

dx
Associate

I want to use STM32N6 with SDMMC1-eMMC as external storage (to store the FSBL and the app). Since eMMC does not support memory mapping, where should the address be selected when using STM32CubeProgrammer to download the bin file? Also, how should the External Loader be configured? Moreover, since eMMC does not support XIP, does that mean only the FSBL+Load&Run mode can be used?

0 REPLIES 0