2020-07-17 1:25 AM
Here is an error:
java -jar STLinkUpgrade.jar
Exception in thread "main" java.lang.UnsatisfiedLinkError: /Users/yes/Downloads/stsw-link007/AllPlatforms/native/mac_x64/libSTLinkUSBDriver.dylib: dlopen(/Users/yes/Downloads/stsw-link007/AllPlatforms/native/mac_x64/libSTLinkUSBDriver.dylib, 1): Library not loaded: @rpath/libusb-1.0.0.dylib
Referenced from: /Users/yes/Downloads/stsw-link007/AllPlatforms/native/mac_x64/libSTLinkUSBDriver.dylib
Reason: image not found
at java.base/java.lang.ClassLoader$NativeLibrary.load0(Native Method)
at java.base/java.lang.ClassLoader$NativeLibrary.load(ClassLoader.java:2452)
at java.base/java.lang.ClassLoader$NativeLibrary.loadLibrary(ClassLoader.java:2508)
at java.base/java.lang.ClassLoader.loadLibrary0(ClassLoader.java:2704)
at java.base/java.lang.ClassLoader.loadLibrary(ClassLoader.java:2637)
at java.base/java.lang.Runtime.load0(Runtime.java:745)
at java.base/java.lang.System.load(System.java:1871)
at com.st.stlinkinterface.e.a(SourceFile:127)
at com.st.stlinkupgrade.app.b.a(SourceFile:62)
at com.st.stlinkupgrade.app.MainApp.main(SourceFile:16)
I also tried to replace provided libusb with installed with brew without luck. So how can I upgrade firmware? Am I missing something?
2020-07-26 11:54 AM
Looks like ST-Link upgrade doesn't work with Java 14, if you have error above just downgrade java to 11.x
2020-08-26 12:09 PM
I am getting the same error. I tried running Java 11.0.8 and Java 8u261, and neither changed anything. Same error. My recently arrived STLINK-V3SET is running firmware V3J1M1B1S1, which is very old. Other suggestions?
2020-08-26 1:47 PM
I was eventually able to upgrade the firmware by running the windows ST-LinkUpgrade.exe from a Windows 10 VirtualBox VM. I found no way to successfully run the Java jar.
2020-10-17 5:42 PM
I had the exact same issue, using Java 8 worked for me.
Might be related to this: https://github.com/AdoptOpenJDK/openjdk-build/issues/1211
Simply downgrading to Java 11 did not work for, but maybe downgrading to 11.0.3 might also work.