cancel
Showing results for 
Search instead for 
Did you mean: 

CH2 on ADC1 does not work while CH15 or CH2+CH15 works fine.

fposser
Associate III

Hi, I did a code to select which channel I want to enable in operation according to some parameters when I start the ADC configuration and TMR.

I have the ADC2 with ch5 and ch10, this work fine, both channels, or only 1 of them.

On ADC1 I have ch2 and ch15, both work fine, only ch15 also, but only ch2 I'm getting strange values on the buffer, more or less 4 times less than what's supposed to be.

Someone have any idea of what's happening?

Thank you!

 

void start_TMR_ADC_DMA(void){
    // Reinitialize the ADCs to start fresh
    MX_ADC1_Init();  // Reinitialize ADC1
    MX_ADC2_Init();  // Reinitialize ADC2

    ADC_ChannelConfTypeDef sConfig = {0};

    // Variables to count the number of active ADC channels
    uint8_t adc1_num_channels = 0;
    uint8_t adc2_num_channels = 0;

    // Configure ADC1 channels based on global variables
    if (adc1_channel_2 == 1) {
        // Enable ADC1 Channel 2
        sConfig.Channel = ADC_CHANNEL_2;
        sConfig.Rank = ADC_REGULAR_RANK_1;
        sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
        sConfig.SingleDiff = ADC_SINGLE_ENDED;
        sConfig.OffsetNumber = ADC_OFFSET_NONE;
        sConfig.Offset = 0;
        sConfig.OffsetSignedSaturation = DISABLE;
        HAL_ADC_ConfigChannel(&hadc1, &sConfig);
        adc1_num_channels++;  // Increment channel count
    }

    if (adc1_channel_15 == 1) {
        // Enable ADC1 Channel 15
        sConfig.Channel = ADC_CHANNEL_15;
        sConfig.Rank = (adc1_num_channels == 1) ? ADC_REGULAR_RANK_2 : ADC_REGULAR_RANK_1;
        sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
        sConfig.SingleDiff = ADC_SINGLE_ENDED;
        sConfig.OffsetNumber = ADC_OFFSET_NONE;
        sConfig.Offset = 0;
        sConfig.OffsetSignedSaturation = DISABLE;
        HAL_ADC_ConfigChannel(&hadc1, &sConfig);
        adc1_num_channels++;  // Increment channel count
    }

    // Configure ADC2 channels based on global variables
    if (adc2_channel_5 == 1) {
        // Enable ADC2 Channel 5
        sConfig.Channel = ADC_CHANNEL_5;
        sConfig.Rank = ADC_REGULAR_RANK_1;
        sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
        sConfig.SingleDiff = ADC_SINGLE_ENDED;
        sConfig.OffsetNumber = ADC_OFFSET_NONE;
        sConfig.Offset = 0;
        sConfig.OffsetSignedSaturation = DISABLE;
        HAL_ADC_ConfigChannel(&hadc2, &sConfig);
        adc2_num_channels++;  // Increment channel count
    }

    if (adc2_channel_10 == 1) {
        // Enable ADC2 Channel 10
        sConfig.Channel = ADC_CHANNEL_10;
        sConfig.Rank = (adc2_num_channels == 1) ? ADC_REGULAR_RANK_2 : ADC_REGULAR_RANK_1;
        sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
        sConfig.SingleDiff = ADC_SINGLE_ENDED;
        sConfig.OffsetNumber = ADC_OFFSET_NONE;
        sConfig.Offset = 0;
        sConfig.OffsetSignedSaturation = DISABLE;
        HAL_ADC_ConfigChannel(&hadc2, &sConfig);
        adc2_num_channels++;  // Increment channel count
    }

    // Set the number of conversions based on the number of enabled channels
    if (adc1_num_channels > 0) {
        hadc1.Init.NbrOfConversion = adc1_num_channels;
        if (adc1_num_channels == 1) {
        	hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
        } else {
        	hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
        }
        HAL_ADC_Init(&hadc1);  // Reinitialize ADC1 to apply the new configuration
    }

    if (adc2_num_channels > 0) {
        hadc2.Init.NbrOfConversion = adc2_num_channels;
        if (adc2_num_channels == 1) {
        	hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
        } else {
        	hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE;
        }
        HAL_ADC_Init(&hadc2);  // Reinitialize ADC2 to apply the new configuration
    }

    // Reinitialize the timers to start fresh
    MX_TIM2_Init();  // Reinitialize TIM2
    MX_TIM3_Init();  // Reinitialize TIM3

    // Start the ADC DMA for both ADCs, ensuring it starts from the beginning of the buffer
    HAL_ADC_Start_DMA(&hadc1, (uint32_t *)adc_i_buffer, ADC_I_BUF_SIZE);  // Start ADC1 DMA
    HAL_ADC_Start_DMA(&hadc2, (uint32_t *)adc_v_buffer, ADC_V_BUF_SIZE);  // Start ADC2 DMA with the first buffer

    // Reset buffer loading state
    v_buf_loaded = 0;

    // Start the timers with interrupts
    HAL_TIM_Base_Start_IT(&htim3);
    HAL_TIM_Base_Start_IT(&htim2);
}
static void MX_ADC1_Init(void)
{

  /* USER CODE BEGIN ADC1_Init 0 */

  /* USER CODE END ADC1_Init 0 */

  ADC_MultiModeTypeDef multimode = {0};
  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC1_Init 1 */

  /* USER CODE END ADC1_Init 1 */

  /** Common config
  */
  hadc1.Instance = ADC1;
  hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
  hadc1.Init.Resolution = ADC_RESOLUTION_16B;
  hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
  hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc1.Init.LowPowerAutoWait = DISABLE;
  hadc1.Init.ContinuousConvMode = DISABLE;
  hadc1.Init.NbrOfConversion = 2;
  hadc1.Init.DiscontinuousConvMode = DISABLE;
  hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T3_TRGO;
  hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
  hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
  hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
  hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
  hadc1.Init.OversamplingMode = DISABLE;
  hadc1.Init.Oversampling.Ratio = 1;
  if (HAL_ADC_Init(&hadc1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure the ADC multi-mode
  */
  multimode.Mode = ADC_MODE_INDEPENDENT;
  if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
/*  sConfig.Channel = ADC_CHANNEL_15;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  sConfig.OffsetSignedSaturation = DISABLE;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
/*  sConfig.Channel = ADC_CHANNEL_2;
  sConfig.Rank = ADC_REGULAR_RANK_2;
  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC1_Init 2 */

  /* USER CODE END ADC1_Init 2 */

}

/**
  * @brief ADC2 Initialization Function
  * @PAram None
  * @retval None
  */
static void MX_ADC2_Init(void)
{

  /* USER CODE BEGIN ADC2_Init 0 */

  /* USER CODE END ADC2_Init 0 */

  ADC_ChannelConfTypeDef sConfig = {0};

  /* USER CODE BEGIN ADC2_Init 1 */

  /* USER CODE END ADC2_Init 1 */

  /** Common config
  */
  hadc2.Instance = ADC2;
  hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
  hadc2.Init.Resolution = ADC_RESOLUTION_16B;
  hadc2.Init.ScanConvMode = ADC_SCAN_ENABLE;
  hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
  hadc2.Init.LowPowerAutoWait = DISABLE;
  hadc2.Init.ContinuousConvMode = DISABLE;
  hadc2.Init.NbrOfConversion = 2;
  hadc2.Init.DiscontinuousConvMode = DISABLE;
  hadc2.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T3_TRGO;
  hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
  hadc2.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
  hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
  hadc2.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
  hadc2.Init.OversamplingMode = DISABLE;
  hadc2.Init.Oversampling.Ratio = 1;
  if (HAL_ADC_Init(&hadc2) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
/*  sConfig.Channel = ADC_CHANNEL_5;
  sConfig.Rank = ADC_REGULAR_RANK_1;
  sConfig.SamplingTime = ADC_SAMPLETIME_16CYCLES_5;
  sConfig.SingleDiff = ADC_SINGLE_ENDED;
  sConfig.OffsetNumber = ADC_OFFSET_NONE;
  sConfig.Offset = 0;
  sConfig.OffsetSignedSaturation = DISABLE;
  if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure Regular Channel
  */
/*  sConfig.Channel = ADC_CHANNEL_10;
  sConfig.Rank = ADC_REGULAR_RANK_2;
  if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN ADC2_Init 2 */

  /* USER CODE END ADC2_Init 2 */

}

 

1 ACCEPTED SOLUTION

Accepted Solutions
fposser
Associate III

My mistake, I change the jumper from SB60 to SB65 and now it's fine.

My jumper configuration of the board was not correct to my usage.

View solution in original post

5 REPLIES 5
STTwo-32
ST Employee

Hello @fposser 

Could you check the errata 2.10.11 of the ES0491. It may be give a discription of the same issue that you are facing.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I will try to configure my ADC in dual mode to see if it fix the problem:

ADC1 and ADC2 are not impacted when running in dual mode, as they operate sampling and conversion at the same time.

 

And it would not explain why when I select only the CH15 or both it works fine. When I select only Ch2 that I have the wrong value.

Andrew Neil
Evangelist III

This is the NUCLEO-H723ZG.

fposser
Associate III

My mistake, I change the jumper from SB60 to SB65 and now it's fine.

My jumper configuration of the board was not correct to my usage.