2020-06-22 7:07 AM
Cannot connect to STM32L05x MCU with CubeProgrammer and ST-Link V3 using the CLI with both "connect under reset" and "Normal" modes. However using the same setup I can connect with ST-Link V2.
Is there any reasoning for this?
2020-06-22 8:10 AM
Select a slower SWD clock rate, try 1 or 4 MHz rather than 24 MHz
Does your interface connect the NRST pin?
2020-06-23 3:44 AM
Yes interface connects to NRST. Clock speed selection doesn't affect it, it will connect in Normal mode but never under reset.
2020-07-07 10:08 AM
I have two IC's that I am working with in this project. STM32L07x and STM32L05x.
With STM32L07x I can connect consistently with ST-LINK V2/V3.
However with STM32L05x it is very inconsistent.
I have tried this with numerous samples of each MCU and have concluded that it must be the MCU compatibility.
Another point to note, I can run STM32L07x in both Normal and under reset mode. With STM32L05x I can only use Normal mode, and even with this it can be very inconsistent.
Any ideas?
2020-07-07 9:16 PM
what voltage the stm32 runs with?
2020-07-08 12:36 AM
3.7V at DCDC which then outputs 1.8V to MCU