2024-11-17 9:10 AM
Hello everyone,
I have designed a custom board with the STM32G0B1CET6N but I cannot connect to the nucleo st-link programmer.
I have removed the two jumpers from the nucleo board but when connecting to the board it doesn't get recognised by the ST-Link Utility or STM32Programmer.
I do get an issue with the driver on the Device Manager but when I connect it to another custom board it works fine.
Below is the schematic for my custom board.
Any help is really appreciated.
Matteo
2024-11-17 9:19 AM
VDDIO2 and VSS on your must be connected too.
2024-11-17 9:23 AM
Hello MM..1,
Thank you for your prompt reply!
Yes, I did noticed that mistake and I have put a temporary cable with the decoupling capacitors. Unfortunately it doesn't seem to work still. I will check that connection again in case there is a bad soldering.
2024-11-17 9:41 AM
Please do yourself a favor. Get a new (and cheap) ST-LINKv3 instead of hacking a nucleo.
2024-11-17 9:46 AM
If it fails so bad the ST-LINK drivers can't find it, you'd need to look at the circuit, for shorts, powering issues, etc.
Check part / connector orientations.
2024-11-17 9:47 AM
Hi Pavel,
Thank you for your reply, I am not actually hacking a nucleo, I am only using the built in st-link to try to program my custom board. I have actually a ST-LinkV3, but I have the same issue.
I am trying to understand what else I am missing, on top of the two connections that MM..1 has nicely pointed out.
Matteo
2024-11-17 10:29 AM
A normal ST-Link at least won't have issues with USB connection to host.
2024-11-17 11:04 AM
Set jumpers back and test link. If work Then show what you disconnect ...
2024-11-17 11:54 AM
Hi MM..1,
Thanks for the reply.
The link is working as normal with jumpers on, also it is working fine with jumpers off on another custom board (L010 chip). I have attached the picture with the jumpers off. I think I need to get a new board done with the VDDIO2 and VSS connected properly as the flying wire maybe are not connected properly. The board was factory assembled so I assume that is right.
BTW....I am new on STM32 so forgive me for silly mistakes.
Matteo
2024-11-17 1:00 PM
For normal use you require three pins connected GND SWCLK SWDIO and on your image GND isnt connected
plus custom board power ...