cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Connect to UART With STM32 Nucleo L476RG

andrewp714
Associate

I just started using and learning how to use the STM32 Nucleo L476RG Board. I am trying to integrate UART into STM32 to display text in Tera Term by using this guide (https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step3_Introduction_to_the_UART).

However, after building and running the project to my board as well as connecting it to Tera Term, output text is still not displaying in Tera Term. I configured my board by activating USART2 with matching default parameters as Tera Term, and is connected to PC through USB A-to-Mini B cable.Screenshot (3).pngScreenshot (4).pngScreenshot (5).pngScreenshot (6).pngScreenshot (7).png Does anyone have a solution? Thanks!

 

3 REPLIES 3
Karl Yamashita
Principal

Check with an oscilloscope to see if the PA2 is transmitting. Then you can determine if it's on the STM32L476 side or VCP/Tera Term side that has an issue.

 

Another thing you can try is to do a loop back test on the VCP. Make sure the STM32 is erased else you won't be able to test the loop back. Place a jumper CN3. You should be able to send some text from Tera Term, and you should see text echo back.

 

KarlYamashita_0-1742600963824.png

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
KnarfB
Principal III

minor thing: use strlen instead of sizeof.

hth

KnarfB

gbm
Principal

Double check the COM port number. In TeraTerm serial config dialog, the bottom panel should display "ST Microelectronics ..."; it doesn't - you are configuring another port in TeraTerm, not the Nucleo VCP.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice