2025-03-22 11:12 AM
Hello
As I am trying to connect the STM32N6570-DK board on the STM32CubeProgrammer, initially the STM32CubeProgrammer recognises my device as in the following picture:
When I press Connect on the STM32CubeProgrammer I get a
warning: Connection to device 0x486 is lost
as in the following picture:
and then an error that says Data read fail
as in the following picture:
I am using a MacBook Air M3, 2024, but even on windows (running on a virtual machine) I get the same error on the STM32CubeProgrammer windows version.
Is there a way to overcome this issue? What could be the cause?
Thank you
2025-03-22 11:49 AM
Hello @Avgerinos
I think this FAQ may help you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-23 2:05 AM
Hello @Avgerinos
I managed to get all STM32Cube tools working on Mac OS M1 and M2 without any issues. I don't have M3 hardware.
Good luck.
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.