2022-05-04 3:35 AM
I made my own PCB with STM32U585AII6Q and there are pins SWCLK, NRST, SWDIO, GND, VDD which I connected to the ST-LINK/V2. When I try to program STM32 U5, I always have error "No device found on target".
Is there a problem with ST-LINK/V2, do I need to use ST-LINK/V3?
Solved! Go to Solution.
2022-05-19 12:03 AM
Thank you!
Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.
2022-05-04 4:56 AM
Hello,
ST-Link V2 works with STM32U585 too.
2022-05-04 6:37 AM
Yes.
Is the board powered? Is a voltage detected in STM32CubeProgrammer?
2022-05-19 12:03 AM
Thank you!
Everything is fine since I programmed STM32U5 via STM32CubeProgrammer.