cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone here sincerely verify my schematic and let me know whether it'll work or not?

Prajnyajit
Associate II

Hi,

I'm mounting STM32L476RGT6U on PCB. For that, I have made this schematic. I need some expert suggestions from anyone who has in-depth knowledge of this. I'll use an ST-LINK V2 to debug and upload the program to the MCU on PCB.

0693W00000FAzVFQA1.jpg

11 REPLIES 11

Have you mounted STM32L476 on PCB? Can you please provide your schematic for STM32L476 so that I can compare and modify mine as per my requirement?

If I need can I order from you?

Paul1
Lead

We used these ST boards before making our own board

  • STM32L476G-EVAL (expensive)
  • STM32L496G-DISCO
  • You can load STM32L476 code onto either of these

Attached example schematic (pdf and DipTrace files)

  • L476_baseV00PR_DipTrace.zip
  • Proprietary circuits removed
  • STLinkV2 with UART (14pin)
  • Option: USB-C VCP
  • Option: DAC for real time diagnostics and
  • Option: Replace DCDC circuit with lower cost option if lower source voltage VH.
  • Option: LEDs and switches powered from 3V3, change resistors appropriately, careful of required voltage for selected LEDs, as indicators 0.1mA is often plenty.
  • RGB LED - Careful: Orientation mark is Pin4 Anode, not pin1. Ensure properly instruct solderer or factory, or delete it.

Paul