2019-11-25 06:31 PM
Using CN4, there are instructions for using an external debug probe to program the on-board STM32G474RE MCU. This seems strange given the fact that there's an embedded ST-LINK/V3, but I've made it work. What I would really like to do is use the embedded ST-LINK/V3 to program an external target via CN4. Unfortunately, there doesn't seem to be any way to disconnect the on-board STM32G474RE from the SWD bus.
Am I overlooking something obvious? Older Nucleo boards had the option of cutting the ST-LINK part of the board off, but the Nucleo-G474RE on my desk doesn't seem to have that option either.
Thanks,
TG
2019-11-25 11:40 PM
2019-11-25 11:56 PM
Ouch. It's so strange that they changed CN4 to the 10-pin connector just so you could program the internal STM32G474 with an external debug probe when the board already comes with a perfectly good ST-LINK/V3 to program it with. Weird.
2024-12-06 07:38 AM