2019-12-09 02:18 AM
Refer to this download page.
In package: en.nucleo-32pins_bom.zip
Everywhere in the document, the wrong uC is mentioned (L412KB)
In package: en.nucleo-32pins_sch.zip
The options for the external oscillator are not shown for STM32L432 (see image)
It seems, that the resources are just copied and pasted... It would be great it anyone could correct these issues.
Best regards!
2019-12-11 12:36 AM
Hello @Pascal Schröer ,
Please note that these resources are shared by all Nucleo 32pins boards.
Your comments are reported internally for farther check, if there is any required update to do.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.