2020-08-02 2:10 PM
After updating CubeIDE to version 1.4.0 (Linux), the debugger does not work.
A window appears
"ST-LINK firmware verification"
in which there is a message - "STLink server is required to launch the debug session".
How to fix it?
2020-08-02 10:58 PM
I downloaded STLINK Server, during installation I received a message that this package is already installed.
Tell me where in CubeIDE are the STLINK Server settings?
2020-08-02 11:59 PM
STM32CubeIDE 1.4.0 debugging works for me on 64-bit Ubuntu 18.04. The stlink-gdb-server comes as a STM32CubeIDE plugin. A typical debug session starts both, arm-none-eabi-gdb (which is on the path in /opt/st/stm32cubeide_1.4.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.4.0.202007081208/tools/bin) and stlink-gdb-server:
$ ps aux | grep -i gdb
frank 28904 0.2 0.0 31968 11968 pts/3 Ss+ 08:40 0:00 arm-none-eabi-gdb --interpreter mi2 --nx -q --interpreter console -ex new-ui mi /dev/pts/2 -ex set pagination off -ex show version
frank 28911 0.7 0.0 34020 4944 ? Sl 08:40 0:00 /opt/st/stm32cubeide_1.4.0/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.linux64_1.4.0.202007081208/tools/bin/ST-LINK_gdbserver -p 61234 -l 1 -d -s -cp /opt/st/stm32cubeide_1.4.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.4.0.202007081208/tools/bin -m 0 -k
Check if those components are installed in your system. If not, I would try reinstalling.
Here is my install log:
$ sudo '/home/frank/Downloads/st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh'
Creating directory st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh.root
Verifying archive integrity... All good.
Uncompressing STM32CubeIDE installer 100%
STMicroelectronics Software License Agreement
...
License accepted.
(Reading database ... 440631 files and directories currently installed.)
Preparing to unpack st-stlink-server-1.3.0-4-linux-amd64.deb ...
stlink-server: no process found
Unpacking st-stlink-server (1.3.0-4) over (1.2.0-3) ...
Preparing to unpack st-stlink-udev-rules-1.0.2-3-linux-all.deb ...
Unpacking st-stlink-udev-rules (1.0.2-3) over (1.0.2-2) ...
Selecting previously unselected package st-stm32cubeide-1.4.0.
Preparing to unpack st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb ...
Unpacking st-stm32cubeide-1.4.0 (1.4.0-7511-20200720-0928-1) ...
Setting up st-stlink-server (1.3.0-4) ...
Setting up st-stlink-udev-rules (1.0.2-3) ...
Setting up st-stm32cubeide-1.4.0 (1.4.0-7511-20200720-0928-1) ...
/
Processing triggers for gnome-menus (3.13.3-11ubuntu1.1) ...
Processing triggers for desktop-file-utils (0.23-1ubuntu3.18.04.2) ...
Processing triggers for mime-support (3.60ubuntu1) ...
Do you want to install Segger J-Link udev rules? [Y/n] n
STM32CubeIDE installed successfully
As a workaround you may switch to ST-Link (OpenOCD) in your Debug Configuration under Debugger.
2020-08-03 12:37 AM
I tried to download STLINK Server from the HELP menu -> Install new software.
Here is the result.
As far as I understand, these elements are present. And the file you specified in the specified path is also there.
I don’t understand what’s the matter ... everything worked before. Ide reinstalled, the result is the same. It works on Windows.
Maybe the paths are not spelled out somewhere?
2020-08-03 12:59 AM
The list of installed packages contains STLINK Server.
2020-08-03 1:01 AM
> Here is the result.
Yes those are outdated versions from last year. The error message is correct.
There should be no need to install STLINK Server separately.
I would try re-installing STM32CubeIDE from scratch.
You first delete all existing versions using
$ sudo apt remove 'st-stm32cubeide*' 'st-stlink*'
and then install the downloaded unzipped shell archive:
$ sudo ~/Downloads/st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh
hth
KnarfB
2020-08-03 1:31 AM
I had exactly the same issue updating to 1.4.0 on Windows. Already tried a clean install and an upgrade to another computer too: nothing worked. Just updated to 1.4.1 and the issue is still present...
Is there any error log we can check to know exactly what's wrong?!
2020-08-03 3:24 AM
I have reinstalled CubeIDE but I will try again on your advice.
I have Arch Linux (Manjaro). I installed the st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.sh package downloaded from the official site.
Sorry for my English, I use a translator ... :)
2020-08-03 3:26 AM
In Windows, this version works, updated to 1.4.1 everything works.
But as for me, the program works more stable on Linux.
2020-08-03 3:30 AM
Actually I didn't know if it was appropriate to post my question here, as this thread explicitly targets Linux. But since the IDE core should be the same I thought at least to ask about some kind of advice on how to get details of what the issue is (eg. server not starting, or whatever). I get nothing more than the "ST-LINK firmware verification" window, all the console/log files are empty...