cancel
Showing results for 
Search instead for 
Did you mean: 

Achieve max timer clock on STM32H7

icethi
Associate II

Hello,

I am trying to achieve the maximum timer clock on the STM32H723ZG for input capturing. In the data sheet is written under Table 4: "The maximum timer clock is up to 550 MHz depending on theTIMPRE bit in the RCC_CFGR register and D2PRE1/2 bits in RCC_D2CFGR register."

I tried to achieve this in the Clock Configuration but it seems like the only solution I found is invalid (see screenshot below). Can I still do that? Or is there another way to do that?

I tried to compile it and it worked without a problem. Sadly I cannot test it on hardware due to delivery.

Thanks in advance!

icethi_0-1707847862612.png

 

 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
STTwo-32
ST Employee

Hello again @Tesla DeLorean @icethi @AScha.3 , thank you for reporting this. I will report this internally to be updated for the next release of the doc. For the Timers mentionned on the table 4 of the datasheet, the maximum frequency is 275MHz.

Best Regards.

STTwo-32 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.