2022-11-07 7:20 AM
I have 11 boards of our prototype with the STM32L4A6AGI6 (i.e. 169 BGA) assembled. 5 of them work fine. The other 6 eventually loose debugging connection. It doesn't happen immediatelly i.e. I'm still able to run a few lines of code but then it resets unrecoverable for the debug session (i.e. I have to restart the entire debug session. Soft reset doesn't work).
I can also measure the NRST (Pin H3) line that is pulled down caused by any internal mechanism (Unhandled interrupt?).
To investigate what line of code is causing the eventually occuring reset I started to place a "while(1);" and checked, if I still can pause and then run again without the debbugger loosing its connection.
This lead me to the following code section:
core_cm4.h
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_TICKINT_Msk |
SysTick_CTRL_ENABLE_Msk;
Removing the "SysTick_CTRL_TICKINT_Msk" my "while(1);" after that line will continue to run without loosing debugging connection. Putting it back again I reach the "while(1);" but eventually it will break.
Now, this may still not be the root of cause. Starting a debugging session and pressing the soft reset button before I even run the program also makes the debugging session crash.
And just to mention again, it works on 5 boards. I.e. it can't really be a firmware issue. But what hardware failure could cause this issue with the above mentioned on the other 6 boards where the error pattern are all the same?
I do have about 10 years experience in the embedded environment dealing with uC quite a lot. But such a constellation I never faced before and causing my brain to blow up soon :face_with_steam_from_nose:.
Any one that may have an idea what is causeing that issue?
Solved! Go to Solution.
2022-11-10 12:13 PM
You are lucky:
it 27 nBOOT0: nBOOT0 option bit (this bit is reserved for STM32L47x/L48x devices)
0: nBOOT0 = 0
1: nBOOT0 = 1
Bit 26 nSWBOOT0: Software BOOT0 (this bit is reserved for STM32L47x/L48x devices)
0: BOOT0 taken from the option bit nBOOT0
1: BOOT0 taken from PH3/BOOT0 pin
2022-11-07 8:13 AM
Hardware checks:
Firmware:
2022-11-07 10:51 AM
This may be one of those cases where the system memory remains mapped at 0x00000000, maybe as consequence of "empty flash bootloader entry" mechanism or improperly connected BOOT0 pin.
JW
2022-11-08 7:53 AM
@Community member
Thx for your input and your check list.
Firmware:
I have programmed the same firmware on all 11 boards. As a firmware is by definition perfect, thus doesn't behave differently if the hardware is the same I would have excluded any wrong doing in the firmware and thus in its configurations. However...
...
phu, well yeah,...
2022-11-08 8:07 AM
@Community member
thx also for your input. This made me check AN2606 and thinking of whats happening if this pin remains floating (which it does, it's not connected anywhere). How ever, as certain boards work reliably and certain reliably not, would fit quite well into this pattern. But would I then be able to debug a single line of code at all? So far, trying to debug it eventually works for a few lines of code until I reach the above described code section (I can provide further details to this if required).
So, somehow yes, but also no. Having it floating I understand that this has to be corrected (pulled up or down)(true?).
... eventually I need anything to be certain what the cause is before I ordere an other batch super expensive boards.
? :dizzy_face:
2022-11-08 8:16 AM
> The boot pin is floating
That is the cause of your problem.
> ... eventually I need anything to be certain what the cause is before I ordere an other batch super expensive boards.
Fix it on the existing boards. If you're lucky, there may be option bits which disable the BOOT0 pin. I don't use the 'L4+.
JW
2022-11-08 8:29 AM
"HSE/Oscillator: I have a 24 MHz external cristal oscilator (FA-128 24.0000MF10Z-W3) that returns a beautiful 0.8 V sine wave."
Datasheet 6.3.7 External clock source characteristics requires max 0.3 to min 0.7 VDDIO for HSE. I do not know your VDDIO, but 0.8 V sine wave seems also not good.
2022-11-08 9:51 PM
One more vote for the BOOT pin!
"Floating" is in general a bad idea for system-determining pins!
Might be a coin toss...
As so many threads here show.
2022-11-10 6:55 AM
Ok, I measured with AC-coppling activated. Using DC-coppling shows that it oscilate between 1.1 V and 1.9 V. As my VDDIO is 3V3 it actually remains outside specs. However, even my good boards don't have more. Additionally, (by mistake) I used so far the internal oscillator as I forgot to activate the external clock in my simplified firmware.
Thus, it has to be checked but it is unfotunatelly still not the cause of the problem.
2022-11-10 7:16 AM
Hehe, "UN"fortuantelly its a 169 pin BGA :> Nope, I made already many electro-surgical intervention to inner layers, but I don't think so that I will be able or nearly successful to get to that pin from the other side.
For sure this is an issue. And it (maybe) explains the issue I have, when starting up the boards that actually work (i.e. when powering it, even with having a voltage supervisor that releases the reset pin not before the voltage reaches 2.9 V, I have to pull down the reset line manually with the attached reset button).
But how would you explain, that I still can run the debugger and run a few lines of codes? I mean, now having this pin floating the uC eventually will detect it as either being "high" or "low". Consequently I would either be able to run it fully functionally and maybe when turning it on a second time it wouldn't work at all, as the BOOT0 eventually makes it decide where to search for the program to run. Wouldn't you agree?
Sorry for insist for further explanation and not simply check that first. The problem is, that I'm unable to rework that on the current board (as visualised above) to check if that helps. I will have to order a new design having this BOOT0 fixed. But as this is going to be expensive in any case, I would want to find a plausible answer to all symtoms before spending the next batch of money. I hope you understand.