cancel
Showing results for 
Search instead for 
Did you mean: 

32F469IDISCOVERY - pre-installed demo not showing on LCD

himsha
Associate II

hello all,

i bought multiple 5 unit of 32F469IDISCOVERY and tested them all not a single one lcd shows pre installed demo. so i bought 2 more uniits from different vender but foud same issue. what would be the possible cause? ia some one got same issue?

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

The issue is not clear. Please decribe the issue in more details..

Is it linked to this thread (I didn't accept the solution in it)?

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Andrew Neil
Super User

Where did you buy them?

have you taken this up with the seller?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
EXUE.2
ST Employee

yes, you are right, for the STM32F469_DK board production from year 2022, we didn't keep demo in the Flash, so you can't see the demo and display on LCD. but you can download the examples from STM32 official Cube to test it.