cancel
Showing results for 
Search instead for 
Did you mean: 

RF Mode Sector Security Status

bon
Associate
Posted on September 20, 2016 at 00:41

I am trying to change the sector security status of my RF sectors in I2C mode using the provided m24lr drivers, but it’s not working. Below is my code:

M24LR_SECTOR_SEC sss_write;
M24LR_SECTOR_SEC sss_read;
// unlock sector
sss_write.SectorLock = 0;
// use first password
sss_write.PassCtrl = 1;
// cannot write without password
sss_write.RW_Protection = 0;
NFCTAG_StatusTypeDef status = NDEF_OK;
uint32_t password = 0;
// present password
status = BSP_NFCTAG_GetExtended_Drv()->PresentI2CPassword(password);
wait_ms(1000);
for (int i = 0; i < 
4
; i++)
{
status
= 
BSP_NFCTAG_GetExtended_Drv
()->WriteSSSx((uint8_t)i, &sss_write);
BSP_NFCTAG_GetExtended_Drv()->ReadSSSx((uint8_t) i, &sss_read);
}

I first present the I2C password, which should be 0 because I haven’t changed it since receiving it. Afterward, I use the m24lr functions to write/read each sector’s SSS. However, even though the code runs and the status is always NDEF_OK, the sector security statuses never change. How can I fix this? I am using the Nucleo-NFC02A1 tag, which uses M24LR04E-R.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Rene Lenerve
ST Employee
Posted on September 20, 2016 at 14:12

Hello on.brian,

There is a bug in the

PresentI2CPassword

function (located in Drivers/BSP/Components/M24LR/m24lr.c)

NFCTAG_StatusTypeDef M24LR_i2c_PresentI2CPassword( const uint32_t PassWord )

{

uint8_t ai2c_message[9] = {0};

uint8_t i;

/* Build I2C Message with Password + Validation code 0x09 + Password */

ai2c_message[4] = 0x09;

i = 0;

while( i <

4

)

{

ai2c_message[i] = ( PassWord >> (i * 8) ) & 0xFF;

ai2c_message[i + 5] = ( PassWord >> (i * 8) ) & 0xFF;

i++;

};

/* Present password to M24LR */

return M24LR_i2c_WriteRegister( ai2c_message, M24LR_I2C_PWD_REG, 9 );

}

th

e M24LR_i2c_WriteRegister function is used to write data to a register. To fix your problem you just have to replace the last line of this function with:   return M24lr_IO_MemWrite( ai2c_message, M24LR_ADDR_SYST_I2C, M24LR_I2C_PWD_REG, 9 );

 and the present password function should work.

We will fix it in a next release.

Second point, you need to initialize the driver pointer by using the init function before using any M24LR functions: (for example)

/* Init M24LR driver */

while( BSP_NFCTAG_Init( ) != NFCTAG_OK );

I hope this will help you,

kind regards.

View solution in original post

2 REPLIES 2
Rene Lenerve
ST Employee
Posted on September 20, 2016 at 14:12

Hello on.brian,

There is a bug in the

PresentI2CPassword

function (located in Drivers/BSP/Components/M24LR/m24lr.c)

NFCTAG_StatusTypeDef M24LR_i2c_PresentI2CPassword( const uint32_t PassWord )

{

uint8_t ai2c_message[9] = {0};

uint8_t i;

/* Build I2C Message with Password + Validation code 0x09 + Password */

ai2c_message[4] = 0x09;

i = 0;

while( i <

4

)

{

ai2c_message[i] = ( PassWord >> (i * 8) ) & 0xFF;

ai2c_message[i + 5] = ( PassWord >> (i * 8) ) & 0xFF;

i++;

};

/* Present password to M24LR */

return M24LR_i2c_WriteRegister( ai2c_message, M24LR_I2C_PWD_REG, 9 );

}

th

e M24LR_i2c_WriteRegister function is used to write data to a register. To fix your problem you just have to replace the last line of this function with:   return M24lr_IO_MemWrite( ai2c_message, M24LR_ADDR_SYST_I2C, M24LR_I2C_PWD_REG, 9 );

 and the present password function should work.

We will fix it in a next release.

Second point, you need to initialize the driver pointer by using the init function before using any M24LR functions: (for example)

/* Init M24LR driver */

while( BSP_NFCTAG_Init( ) != NFCTAG_OK );

I hope this will help you,

kind regards.

bon
Associate
Posted on September 20, 2016 at 19:26

That fixed it! Thank you.