cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with reconnect to board after power down

Tal.Ram
Associate II
Posted on August 18, 2016 at 07:58

Hi, we're using the MB1054A board for reading ISO 15693 tags and it works OK.

the problem occurs after immediate power down- we are facing problems with initiation.

The OS on the PC is Win-10 and we're not sure the CR95HF.dll is the same used on the application SW. how come when shut down the PC and power up again, and then open again the application SW everything is working OK?

Do ST supply source code example for the PC side? 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on August 23, 2016 at 15:37

Hi,

I need more details to be able to reproduce the issue : I understand that the initiation doesn't work after power down. What do you mean about Initiation ? is it MB1054A power down, software power down or computer power down ?

About source code example :

you can read Application Note AN3954 that explain how to develop software to drive M1054A board :

http://www.st.com/content/ccc/resource/technical/document/application_note/50/3e/09/39/51/a5/4c/3d/DM00034558.pdf/files/DM00034558.pdf/jcr:content/translations/en.DM00034558.pdf

Also available, source code examples (C & VB6) : 

http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-95hf002.html

Best regards

ST support

View solution in original post

2 REPLIES 2
Posted on August 23, 2016 at 15:37

Hi,

I need more details to be able to reproduce the issue : I understand that the initiation doesn't work after power down. What do you mean about Initiation ? is it MB1054A power down, software power down or computer power down ?

About source code example :

you can read Application Note AN3954 that explain how to develop software to drive M1054A board :

http://www.st.com/content/ccc/resource/technical/document/application_note/50/3e/09/39/51/a5/4c/3d/DM00034558.pdf/files/DM00034558.pdf/jcr:content/translations/en.DM00034558.pdf

Also available, source code examples (C & VB6) : 

http://www.st.com/content/st_com/en/products/embedded-software/st25-nfc-rfid-software/stsw-95hf002.html

Best regards

ST support

Tal.Ram
Associate II
Posted on August 28, 2016 at 08:52

Hi,

The power down reffers to computer sudden shut down.

After power up of the computer we have problems with proper readings of the tags.

We think it's CR95HF.dll problem and the examples of the source codes are not sufficient.

How come when using one of the eval SW, after PC shut down and power up, and then re-open the SW- the data of the tag is being read OK?

We must understand this issue because other solution is to use other board with proper SDK.