2024-07-16 08:12 PM
Hi,
I want to operate reader board in CE mode.
I posted the question before and I got the resolution from STSW-ST25R016 library.
I have more questions about ndef_type_wifi.h file.
Looking at the header file, you support it as below, but I would like to check the value of the macro again.
Is it correct value?
And is the type after the written version not supported? (ex. wpa3, sae, etc.)
#define NDEF_WIFI_AUTHENTICATION_NONE 0U /*!< WPS No Authentication (Should be 1, but set to 0 for Android native support) */
#define NDEF_WIFI_AUTHENTICATION_WPAPSK 2U /*!< WPS Authentication based on WPAPSK */
#define NDEF_WIFI_AUTHENTICATION_SHARED 3U /*!< WPS Authentication */
#define NDEF_WIFI_AUTHENTICATION_WPA 4U /*!< WPS Authentication based on WPA */
#define NDEF_WIFI_AUTHENTICATION_WPA2 5U /*!< WPS Authentication based on WPA2 */
#define NDEF_WIFI_AUTHENTICATION_WPA2PSK 6U /*!< WPS Authentication based on WPA2PSK */
#define NDEF_WIFI_ENCRYPTION_NONE 0U /*!< WPS No Encryption (Should be 1, but set to 0 for Android native support) */
#define NDEF_WIFI_ENCRYPTION_WEP 2U /*!< WPS Encryption based on WEP */
#define NDEF_WIFI_ENCRYPTION_TKIP 3U /*!< WPS Encryption based on TKIP */
#define NDEF_WIFI_ENCRYPTION_AES 4U /*!< WPS Encryption based on AES */
Best regards,