2022-03-22 09:30 PM
In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing
Solved! Go to Solution.
2022-03-23 01:36 AM
Hi,
ST25R readers such as
can be used to communicate with ST25DV Dynamic tags.
For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.
The ST25PC-NFC application provides access to the various features of the ST25DV tags
Rgds
BT
2022-03-22 09:32 PM
In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing purposes? PC based application is necessary to read/write the data.
2022-03-23 01:36 AM
Hi,
ST25R readers such as
can be used to communicate with ST25DV Dynamic tags.
For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.
The ST25PC-NFC application provides access to the various features of the ST25DV tags
Rgds
BT