cancel
Showing results for 
Search instead for 
Did you mean: 

NFC reader supporting ST25DV

KKulk.1
Associate

In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

ST25R readers such as

can be used to communicate with ST25DV Dynamic tags.

For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.

The ST25PC-NFC application provides access to the various features of the ST25DV tags

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KKulk.1
Associate

In our project, we are using ST micro NFC chip (ST25DV). So, the query is which card Reader be supported to read/write data for ST micro NFC chip (ST25DV)? Secondly, which PC-based applications can be used to see the data after reading or writing purposes? PC based application is necessary to read/write the data.

Brian TIDAL
ST Employee

Hi,

ST25R readers such as

can be used to communicate with ST25DV Dynamic tags.

For the PC based application, I would recommend to use the ST25PC-NFC Windows® PC software with either a Discovery kit for the ST25R3916 or with a Discovery kit for the ST25R3911B.

The ST25PC-NFC application provides access to the various features of the ST25DV tags

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.