cancel
Showing results for 
Search instead for 
Did you mean: 

Lock write access on ST25DV04K using ST25R3916

cmsilva
Associate

I'm fairly new in NFC technology and was trying to implement a simple project that uses the ST25R3916 to write a message in a specific memory location of the ST25DV04K and then locks write access to that specific memory location. I'm using an adapted version of the library "en.x-cube-nfc6". I can read/write messages without any problem, but when I can't seem to find any function in the library to block the write access that works. I'm using  "ndefPollerWriteBytes(ndefContext *ctx, uint32_t offset, const uint8_t *buf, uint32_t len)" to write, which works fine, butif I try to use "ndefPollerSetReadOnly(ndefContext *ctx)", it returns error 33 "Wrong State". Am I doing something wrong? Should I use different functions? I'll append a picture of my code, which stems from the demo usage of the library. The purpuse of the code was to write 4 bytes, lock access then try to write again (which sould fail, I guess).

code.jpeg

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

ndefPollerSetReadOnly is supposed to be used on tags being in READ/WRITE state. I guess your tag is in INITIALIZED state. As you directly write raw data into the tag memory with ndefPollerWriteBytes (i.e. you did not write a formatted NDEF message), the ctx->state (tag state) stays at value NDEF_STATE_INITIALIZED and makes ndefPollerSetReadOnly returns ERR_WRONG_STATE. You can either write a message with an empty NDEF to move to NDEF_STATE_READWRITE before calling ndefPollerSetReadOnly or force the ctx->state value to NDEF_STATE_READWRITE.

Note that the support of the Lock Block command is optional for tags. For ST25DV04K tags, this command is only applicable for the blocks 0 and 1 (see ST25DV datasheet). 

For your use case, I would rather suggest to use data protection (see section 5.6). The API needed for the data protection are available in rfal_st25xv.c (e.g. rfalST25xVPollerPresentPassword).

 

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

Hi,

ndefPollerSetReadOnly is supposed to be used on tags being in READ/WRITE state. I guess your tag is in INITIALIZED state. As you directly write raw data into the tag memory with ndefPollerWriteBytes (i.e. you did not write a formatted NDEF message), the ctx->state (tag state) stays at value NDEF_STATE_INITIALIZED and makes ndefPollerSetReadOnly returns ERR_WRONG_STATE. You can either write a message with an empty NDEF to move to NDEF_STATE_READWRITE before calling ndefPollerSetReadOnly or force the ctx->state value to NDEF_STATE_READWRITE.

Note that the support of the Lock Block command is optional for tags. For ST25DV04K tags, this command is only applicable for the blocks 0 and 1 (see ST25DV datasheet). 

For your use case, I would rather suggest to use data protection (see section 5.6). The API needed for the data protection are available in rfal_st25xv.c (e.g. rfalST25xVPollerPresentPassword).

 

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.