2019-07-18 12:17 AM
I have the X-Nucleo-NFC30A1 with the Cr95HF chip. My question is: Is the Listen Mode supported for Type A tags?
I used the X-Cube-NFC3 v2.0.0 and managed to get the Tag Detector working. But I am trying to implement the Listen Mode and am facing problems. When I build the project by making changes to the platform.h as:
#define RFAL_FEATURE_ISO_DEP_LISTEN true
and
#define RFAL_FEATURE_LISTEN_MODE true
I get undefined references to st25r95Listen, st25r95RearmListen and st25r95SPIGetLmState. Any suggestions would be helpful.
Thank You.
Solved! Go to Solution.
2019-07-18 02:31 AM
Hi,
thanks for using ST25R95/CR95HF product. Card Emulation source code is not part of the X-CUBE-NFC3 v2.0.0 but I will provide it to you.
An updated version of the RFAL for ST25R95/CR95HF is also available in STSW-ST25RFAL003. I would suggest to upgrade to this version (i.e. to replace RFAL files from X-CUBE-NFC3 with the new ones).
Feel free to share more details about your card emulation application so that I can provide right support to you.
Thanks
Rgds
BT
2019-07-18 02:31 AM
Hi,
thanks for using ST25R95/CR95HF product. Card Emulation source code is not part of the X-CUBE-NFC3 v2.0.0 but I will provide it to you.
An updated version of the RFAL for ST25R95/CR95HF is also available in STSW-ST25RFAL003. I would suggest to upgrade to this version (i.e. to replace RFAL files from X-CUBE-NFC3 with the new ones).
Feel free to share more details about your card emulation application so that I can provide right support to you.
Thanks
Rgds
BT