cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use only the UART interface of the ST25R3911B-DISCO instead of the USB?

ESobr
Associate

I'm using a ST25R3911B-DISCO for a project and I need to use the UART interface, instead of the USB one and the software provided by ST, to send commands (like INVENTORY, READ BLOCK, WRITE BLOCK) and receive the corresponding information.

Is it possible with this board? And if it is, how can I proceed to implement it?

Thanks in advance,

Eduardo

10 REPLIES 10
sener
Associate II

I like to share one of my experience with ST25R3911B-DISCO.

We have an implementation requiring to read 5 by 5 cm label RFID tags glued (no more that 0.3mm thickness) onto a massive (3cm thickness) aluminum metal block. And that device can still read it although the distance is just max. 2cm which is still good enough for the task.