2014-05-26 2:23 PM
What is the recommended way to mange simultaneous I�C and RF data transfers with M24SR IC and 2 Host MCU & NFC Phone?
I have implemented mechanism with time Slice , so that each Host has time window to communicate with the M24SR , but still have some issues to resolve , such as the size of Time Slice , number of retry etc. if anyone has better idea i will appreciate very much . #m24sr #session #rf #rf-session #gpo #i2c #i2c #m24srSolved! Go to Solution.
2014-06-10 6:38 AM
Hello ,
1)
Priority management will wait completion of RF command before shutting RF session and open I2C session .
2)
M24SR could only have two host families , one RF and one I2C and management is performed between RF and I2C .
Playing with GPO in session mode you can imagine to have several I2C host addressing the same M24SR
I hope this is helping you,Best regards,ST dynamic NFC/RFID tags e2e support2014-06-02 2:59 AM
M24SR was built around the session mechanism which can affect the communication to one or other protocol .
On top of that I2C has super user priority and can cancel RF session if necessary .
In conclusion best way to manage M24SR is to use the session mechanism .
I hope this is helping you, Best Regards, Have a nice day, ST NFC/RFID dynamic tag e2e support2014-06-09 10:34 AM
Thanks for the Quick Reply , few open issue :
1.If using I2C super user , it can kill ongoing RF Session this can lead to data corruption 2.the Session mechanism force the M24SR to give the attention to the first Host that request to open session , it doesnt deal with multiple Host .What i am asking for, how to manage two Host Communicating with M24SR Periodically ?2014-06-10 6:38 AM
Hello ,
1)
Priority management will wait completion of RF command before shutting RF session and open I2C session .
2)
M24SR could only have two host families , one RF and one I2C and management is performed between RF and I2C .
Playing with GPO in session mode you can imagine to have several I2C host addressing the same M24SR
I hope this is helping you,Best regards,ST dynamic NFC/RFID tags e2e support