cancel
Showing results for 
Search instead for 
Did you mean: 

HALT only single tag in field

RMuiz.1
Associate III

Hi!

I have a case where I want to read all tags in area one by one. Issue is that if I call `HLTA` command, even after selecting a tag, all tags in area go to sleep. Is this intended behavior in ISO 14443A protocol or I am doing something wrong?

Hlta -> https://github.com/jspngh/st25r3911b/blob/master/src/lib.rs#L275
Select -> https://github.com/xpresshd/st25r3911b/blob/master/src/lib.rs#L575

Thanks!

 

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

1. Yes
2. Yes

Now with field restart before WUPA it works as I intended.

Currently I send `Reset` command to turn off field. I was wondering if there is a cleaner way to do it. No field off commands? :)

Hi,

our RFAL rfalFieldOff API just clears the rx_en and tx_en bits in the Operation control register.

 

Rgds

BT

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.