cancel
Showing results for 
Search instead for 
Did you mean: 

For nfc reader can you suggest smd antenna

PMK.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Travis Palmer
ST Employee

Hello,

there are different types of antennas.

For all types of antennas the self resonance frequency should be above 13.56MHz. (typically between 40MHz - 120MHz). The matching network is then used to make them resonating at 13.56MHz and therefore suite able for NFC. Also the Q-factor should be in a decent range, dependent on used technology and bitrate. AN5276 is providing a good overview about important antenna parameters.

Selecting the right antenna depends in most cases on the overall system and use-case. In an access control reader, a smd antenna could maybe also be used to read an ID1 tag, but the read range and cost might not be satisfying.

BR Travis

View solution in original post

1 REPLY 1
Travis Palmer
ST Employee

Hello,

there are different types of antennas.

For all types of antennas the self resonance frequency should be above 13.56MHz. (typically between 40MHz - 120MHz). The matching network is then used to make them resonating at 13.56MHz and therefore suite able for NFC. Also the Q-factor should be in a decent range, dependent on used technology and bitrate. AN5276 is providing a good overview about important antenna parameters.

Selecting the right antenna depends in most cases on the overall system and use-case. In an access control reader, a smd antenna could maybe also be used to read an ID1 tag, but the read range and cost might not be satisfying.

BR Travis