Hello Gilles,Typically the NFC antenna is not touchable. Thinking about access reader or EMVCo payment terminals, the NFC antenna is several mm below the surface, covered by plastic or any other material and not touchable. Thus an electrostatic disch...
Hello Rob_Talor, Bypassing the internal regulator means, connecting the VDD_DR/RF directly to VDD_Tx. On the MB1414-B this can be done by closing J206. AS stated in the Absolute maximum ratings table: "Peak current supplied from an external source, i...
Hello Huzaifa_Tariq01,I would then recommend to split the power supply for the hall sensors and the NFC section (maybe add an additional LDO) to increase PSRR and split the grounds.As Ascha.3 highlighted, a current flowing on a common ground track ca...
Hello Huzaifa_Tariq01,If I understood your post correctly, you assume that the NFC reader is disturbing the hall sensors.Hall sensor are based on magnetic sensing. In your setup, can they be disturbed by the magnetic field sent by the ST25R device?Yo...