2020-12-04 9:09 AM
I originaly added the CubeMX NFC firmware module and made a few builds with that library.
Then I removed the NFC component and now every time I generate the code the folders lib_nfc\Target and lib_nfc are added to project resulting in a few warning.
I have to manualy remove the paths from build settings, but every code generation they are added again.
Someone can indicate me where I can switch off this behavior?
Solved! Go to Solution.
2020-12-14 3:06 AM
Thank you for the answer.
I already did some investigationbefore resorting to the forum, and unfortunately there is no mention of lib_nfc in .ioc file.
In .cproject file there is the path actually added back during code generation.
Non mention of lib_nfc in the registry too.
But your suggestion made me try another more aggressive approach:
I ran a "grep -r lib_nfc *.*" in the root folder of the project ...
I found a mention of lib_nfc deep inside a .metadata binary file that I couldn't change.
But also an additional reference of the lib_nfc inside the .cproject file in an obscure entry:
<option id="com.st.stm32cube.ide.mcu.gnu.managedbuild.option.defaults.1897218958" ...
far to the right and several screens off side, intermixed with other (legitimate?) project folders.
Manually removing those entries fixed the problem.
Thank you.
2020-12-04 2:34 PM
Either CubeMX is in a weird/buggy state due to you adding and then removing a component, or you're missing something within the configuration. If you can share the IOC, someone may take a look. You make be able to open the IOC itself in a text editor and see/fix the issue.
2020-12-14 3:06 AM
Thank you for the answer.
I already did some investigationbefore resorting to the forum, and unfortunately there is no mention of lib_nfc in .ioc file.
In .cproject file there is the path actually added back during code generation.
Non mention of lib_nfc in the registry too.
But your suggestion made me try another more aggressive approach:
I ran a "grep -r lib_nfc *.*" in the root folder of the project ...
I found a mention of lib_nfc deep inside a .metadata binary file that I couldn't change.
But also an additional reference of the lib_nfc inside the .cproject file in an obscure entry:
<option id="com.st.stm32cube.ide.mcu.gnu.managedbuild.option.defaults.1897218958" ...
far to the right and several screens off side, intermixed with other (legitimate?) project folders.
Manually removing those entries fixed the problem.
Thank you.