2018-06-19 02:04 AM
Our new products have the ST25DV04K on board to identify them. We can read the NFC chip with our android phones. But the ACR122 from ACS doesn't detect the NFC.
I tested the ACR122 with the X-NUCLEO-NFC01A1 and the X-NUCLEO-NFC04A1. The first one works fine, but the second one with the ST25 is also not detected by the ACR122.
Can you help us with this problem? Thanks
#st25dv04k #st25 #acr #acr122 #nfcSolved! Go to Solution.
2018-06-20 01:39 AM
Hi Joris,
as described on ACS internet web site :
'The
is a PC-linked contactless smart card reader/writer developed based on 13.56 MHz Contactless (RFID) Technology. Compliant with the ISO/IEC18092 standard for Near Field Communication (NFC), it supports not only MIFARE® and ISO 14443 A and B cards, but also all four types of NFC tags.'X-NUCLEO-NFC01A1 is based on M24SR series that is ISO14443-A RF protocol and is supported by ACR122 reader.
X-NUCLEO-NFC04A1 is based on ST25DV-I2C series that is ISO15693 / NFC TYPE5 RF protocol that is not supported by ACR122 reader.
This is the reason why ACR122 reader can be used with X-NUCLEO-NFC04A1. You need to select a reader supporting ISO15693 / NFC TYPE5 RF protocol.
Best regards
NFC/RFID ST support
2018-06-20 01:39 AM
Hi Joris,
as described on ACS internet web site :
'The
is a PC-linked contactless smart card reader/writer developed based on 13.56 MHz Contactless (RFID) Technology. Compliant with the ISO/IEC18092 standard for Near Field Communication (NFC), it supports not only MIFARE® and ISO 14443 A and B cards, but also all four types of NFC tags.'X-NUCLEO-NFC01A1 is based on M24SR series that is ISO14443-A RF protocol and is supported by ACR122 reader.
X-NUCLEO-NFC04A1 is based on ST25DV-I2C series that is ISO15693 / NFC TYPE5 RF protocol that is not supported by ACR122 reader.
This is the reason why ACR122 reader can be used with X-NUCLEO-NFC04A1. You need to select a reader supporting ISO15693 / NFC TYPE5 RF protocol.
Best regards
NFC/RFID ST support