cancel
Showing results for 
Search instead for 
Did you mean: 

about X-NUCLEO-NFC06A1 and STM32F401RE nucleo board

DSai.1
Associate III

Dear Sir,

In order to check the RFAL functions with sample project in ST25NFC_Embedded_Lib_ST25R3916_1.4.0\Projects\STM32L476RG-Nucleo\Applications,

I bought a X-NUCLEO-NFC06A1. I have a STM32F401RE nucleo board already, I wonder

if the two board can be used for checking function without any modification of the sample code.

If any modification is necessary, would you like to inform me the related information.

best regards

Dai Sai

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

Hi,

projects in ST25NFC_Embedded_Lib_ST25R3916_1.4.0 can be directly used on NUCLEO-L476RG.

For other Nucleo boards, a porting is needed (see tutorial in https://community.st.com/s/question/0D53W00001Px5sKSAR/how-to-create-a-project-with-x-cube-nfc06).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
DSai.1
Associate III

I plan to use STM32CubeIDE for checking. I installed the STM32CubeIDE for window,

but can not find any project file with "Import Project" selection.

any help for me?

best regards

Dai Sai

Brian TIDAL
ST Employee

Hi,

projects in ST25NFC_Embedded_Lib_ST25R3916_1.4.0 can be directly used on NUCLEO-L476RG.

For other Nucleo boards, a porting is needed (see tutorial in https://community.st.com/s/question/0D53W00001Px5sKSAR/how-to-create-a-project-with-x-cube-nfc06).

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DSai.1
Associate III

Dear Brain,

thank you for your reply. It seems my environment is good for checking function now.

If necessary, I will try to use STM32CubeIDE.

best regards

Dai Sai