cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IHM03A1 max voltage

Ben S
Associate II

Why is the input voltage of the X-NUCLEO-IHM03A1 dev board limited to 50V? Looking at the schematic and BOM I don't see any reason why it shouldn't be 85V.

This question has been asked before but didn't receive a clear answer.

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @Ben S​ and welcome to the ST Community.

The board has been validated up to the declared operating voltage.

Use at higher voltages is possible, but the board has not been tested.

If you feel a post has answered your question, please click "Accept as Solution"