cancel
Showing results for 
Search instead for 
Did you mean: 

X_NUCLEO_IHM02A1 with Raspberry Pi 4B. Can anybody help me with the links between these boards?

ALupo.1
Associate

Also, the red led of IHM02A1 is On all the time .Is this normal?Thank you.

1 REPLY 1
Cristiana SCARAMEL
ST Employee

Hello @ALupo.1​ and welcome to the ST Community.

The red LED indicates that at least one of the two devices is in fault condition.

As described in the L6470 datasheet at the end power-up, the FLAG output is forced low.

It is necessary to send a GetStatus command to reset the STATUS register flags.

Let me know if this info help you.