cancel
Showing results for 
Search instead for 
Did you mean: 

Wireless Charging solution Wiki

willzhou
ST Employee

This Topic is used for Wireless Charging solution

1.Mcu C drive code:

GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs

willzhou_0-1717985741931.png

2. Python drive code, check attach file "Python_FT260_ST_WLC.7z"

STwirelesscharger/Python_FT260_ST_WLC: use FT260 dongle and operate ST wireless charge chips

 

3. If your wlc chip i2c is ok but GUI can not connected, please use wlc_ft260_Recovery tool, check attach file "wlc_ft260_Recovery.7z"

4. STWBC2 console log capture tool "STWBC2_tools.7z"

5. STSW-WPSTUDIO Tool: STwirelesscharger/STSW-WPSTUDIO: ST wireless charge chip tool (github.com)

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
14 REPLIES 14
willzhou
ST Employee

STEVAL-WLC38RX check attach "STEVAL-WLC38RX.zip" file, include blow

DB5040Wireless power receiver evaluation board for Qi BPP/EPP applications
AN5961Wireless power transfer coil design
UM3154Getting started with the STEVAL-WLC38RX wireless power receiver evaluation board for 5 W Qi BPP and 15 W Qi EPP applications
STEVAL-WLC38RX GERBER
STEVAL-WLC38RX BOM
STEVAL-WLC38RX SCHEMATIC

STDES-WLC38TWS check attach "STEVAL-WLC38TWS.zip" file, include blow

DB4898 Qi-1.3 compatible wireless power receiver reference design for 2.5W True Wireless Stereo (TWS) applications
TN1441STDES-WLC38TWS wireless power receiver quick start guide and test report
STDES-WLC38TWS GERBER
STDES-WLC38TWS BOM
STDES-WLC38TWS SCHEMATIC
DB4944 Firmware for STDES-WLC38WA and STDES-WLC38TWS wireless charger receiver evaluation kit

STDES-WLC38WA check attach "STEVAL-WLC38WA.zip" file, include blow

DB4897Qi-1.3 compatible wireless power receiver reference design for 2.5W wearable applications
TN1440STDES-WLC38WA wireless power receiver quick start guide and test report
STDES-WLC38WA GERBER
STDES-WLC38WA BOM
STDES-WLC38WA SCHEMATIC
DB4944Firmware for STDES-WLC38WA and STDES-WLC38TWS wireless charger receiver evaluation kit

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

STEVAL-WBC86TX see attach "STEVAL-WBC86TX.zip" file, include below:

DB5000Qi-compatible wireless power transmitter evaluation board for 5 W application based on STWBC86
AN5961Wireless power transfer coil design
UM3161Getting started with the STEVAL-WBC86TX wireless power transmitter evaluation board for up to 5 W Qi-BPP applications
STEVAL-WBC86TX GERBER
STEVAL-WBC86TX BOM
STEVAL-WBC86TX SCHEMATIC
DB4883Firmware for STEVAL-WBC86TX wireless charger transmitter evaluation kit

mcu driver code

GitHub - STMicroelectronics/STWirelessCharging-C-Drivers: Standard C platform-independent drivers for wireless charging ICs

python driver code see "python_ft260_st_wbc86.7z" file

add bidi python code see "ST_WLC_SampleCode_python_v1.03.zip"

STWBC86 use for bi-directional communication - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

STEVAL-WLC99RX see attach "STEVAL-WLC99RX.zip" file, include below

DB5088 and UM3262, Sch and PCB

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

STEVAL-WBC2TX50 check attach "STEVAL-WBC2TX50.zip" file, include DB5125 and UM3231, Sch and PCB

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
willzhou
ST Employee

STEVAL-WBC2TX70 check attach "STEVAL-WBC2TX70.zip" file

FW: STSW-WBC2FW_V1300.7z

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STSW-WPSTUDIO

GitHub - STwirelesscharger/STSW-WPSTUDIO: ST wireless charge chip tool

UM3164 STSW-WPSTUDIO user guide: “UM3164 STSW-WPSTUDIO user guide.pdf”

willzhou_0-1721034562772.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, most of the links do not work anymore...

sean123
Associate

There is currently an issue with the ST website. The website will not load the "Product selector" and "Documentation" tabs on the wireless charging page. Datasheet links are not working for STWLC38 and STWLC98, among others. Links to some eval boards are also serving 404 errors

The document is being updated, and once the update is complete, a new link will be provided.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.