2024-06-09 6:40 PM - edited 2025-03-28 7:35 AM
This Topic is used for Wireless Charging solution
1.Mcu C drive code:
2024-06-09 6:44 PM - edited 2024-11-16 11:12 PM
STEVAL-WLC38RX check attach "STEVAL-WLC38RX.zip" file, include blow
DB5040Wireless power receiver evaluation board for Qi BPP/EPP applications
AN5961Wireless power transfer coil design
UM3154Getting started with the STEVAL-WLC38RX wireless power receiver evaluation board for 5 W Qi BPP and 15 W Qi EPP applications
STEVAL-WLC38RX GERBER
STEVAL-WLC38RX BOM
STEVAL-WLC38RX SCHEMATIC
STDES-WLC38TWS check attach "STEVAL-WLC38TWS.zip" file, include blow
DB4898 Qi-1.3 compatible wireless power receiver reference design for 2.5W True Wireless Stereo (TWS) applications
TN1441STDES-WLC38TWS wireless power receiver quick start guide and test report
STDES-WLC38TWS GERBER
STDES-WLC38TWS BOM
STDES-WLC38TWS SCHEMATIC
DB4944 Firmware for STDES-WLC38WA and STDES-WLC38TWS wireless charger receiver evaluation kit
STDES-WLC38WA check attach "STEVAL-WLC38WA.zip" file, include blow
DB4897Qi-1.3 compatible wireless power receiver reference design for 2.5W wearable applications
TN1440STDES-WLC38WA wireless power receiver quick start guide and test report
STDES-WLC38WA GERBER
STDES-WLC38WA BOM
STDES-WLC38WA SCHEMATIC
DB4944Firmware for STDES-WLC38WA and STDES-WLC38TWS wireless charger receiver evaluation kit
2024-06-09 6:44 PM - edited 2025-03-28 7:35 AM
STEVAL-WBC86TX see attach "STEVAL-WBC86TX.zip" file, include below:
DB5000Qi-compatible wireless power transmitter evaluation board for 5 W application based on STWBC86
AN5961Wireless power transfer coil design
UM3161Getting started with the STEVAL-WBC86TX wireless power transmitter evaluation board for up to 5 W Qi-BPP applications
STEVAL-WBC86TX GERBER
STEVAL-WBC86TX BOM
STEVAL-WBC86TX SCHEMATIC
DB4883Firmware for STEVAL-WBC86TX wireless charger transmitter evaluation kit
mcu driver code
2024-06-09 6:45 PM - edited 2024-11-16 11:00 PM
2024-06-09 6:46 PM - edited 2024-11-16 11:01 PM
2024-06-09 6:46 PM - edited 2024-11-16 11:03 PM
2024-07-15 2:11 AM - edited 2025-03-10 10:59 PM
STSW-WPSTUDIO
UM3164 STSW-WPSTUDIO user guide: “UM3164 STSW-WPSTUDIO user guide.pdf”
2024-08-12 12:29 AM
Hi, most of the links do not work anymore...
2024-08-18 1:55 AM
The document is being updated, and once the update is complete, a new link will be provided.
2024-09-05 5:24 AM
it's been a few weeks and it appears the documents are still temporarily unavailable. I managed to get most of the relevant PDFs using the wayback-machine but the Gerber zip-files are not hosted there. @willzhou, would you be willing to email/post the Gerber files for the steval-wlc38rx, or any of the reference designs (stdes-wlc38wa or stdes-wlc38tws-bom) for the STWLC38 (or other ICs)?
I'm asking because i'm struggling to route all the traces from the BGA footprint. Even with filled+capped vias, some of the middle pads are tricky to fan-out. It seems EuroCircuits wouldn't be capable of producing a sufficiently precise PCB; which manufacturer does ST prefer for its eval boards?