2022-12-01 5:45 AM
I have a STEVAL-IPM05F. My goal is to switch on/off the IGBTs. While I try that, I got many difficulties, like loading the Boots voltage etc. Now I have four questions.
Pls a good answer is very important, because in my last question the answer was wrong and I tried to test the board with that answer and lost a lot of time.
Thank you!
Solved! Go to Solution.
2022-12-15 2:12 AM
After I connected the 3.3V to the correct J2 Pin, I get a voltage between the two ends of the same cable. My control board is connected to my laptop with a galvanic isolation and the laptop is not pluged, the powerboard is connected to a voltage generator (15-20V) and the grounds from the power and control board are connected to each other too. Why am I get a potential difference between pin 28 and 3.3V pin from the control board, when they are connected ?
Thank you
Ismail
2022-12-01 7:33 AM
5V via header
3.3V via header
From User Manual
"The board requires +5 V and +3.3 V to be supplied externally through the 34-pin motor control connector J2. Please refer to the relevant board manuals for information on key connections and supplies."
https://www.st.com/resource/en/schematic_pack/steval-ipm05f_schematic.pdf
2022-12-02 5:07 AM
Ciao
Ciao
Gigi
2022-12-08 12:50 AM
When I look in the manuals, the 34-pin on J2 is the "measure phase C"-pin. This does't make sense to me. Is it possible to explain it, why this is the correct one?
2022-12-08 12:56 AM
2022-12-08 1:29 AM
After I read your answer again I checked that you mean not the 34. pin. Sry! which on of the pin is the Input pin for 3.3/5V? Thank you!
2022-12-12 2:19 AM
Ciao
If the SD pin is 0V even if you provide the signal to turn ON the power switches, they will not turned on (it is a safety feature). Normally this pin is pullup to +3.3V using a resistor, but if you don't provide the +3.3V to the J2 pin 28 this pin will be always zero volt.
Considering the Table 6 of the manual
pin 25 +V power. You have to provide to this pin +5V
pin 28 Vdd_m.You have to provide to this pin the 3.3V
pin 14 HV bus voltage. This is a signal for the microcontroller to monitor the DC bus voltage. In the board is done using the voltage divider composed by R1, R2 and R4
Ciao
Gigi
2022-12-13 3:57 AM
Thank you!
2022-12-15 2:12 AM
After I connected the 3.3V to the correct J2 Pin, I get a voltage between the two ends of the same cable. My control board is connected to my laptop with a galvanic isolation and the laptop is not pluged, the powerboard is connected to a voltage generator (15-20V) and the grounds from the power and control board are connected to each other too. Why am I get a potential difference between pin 28 and 3.3V pin from the control board, when they are connected ?
Thank you
Ismail