2023-11-27 09:36 AM
The datasheet says that
LM211D/DT has a temperature of -40 °C, +105 °C and output to negative supply voltage 50V
LM311D/DT has a temperature of -0 °C, +70 °C and output to negative supply voltage 40V
Is there any differences in performance or electrical characteristics between the two?
2023-11-27 09:57 AM
Welcome @jgananam, to the community!
No, there are no differences in performance.
Good luck!
/Peter